OMRON at ISE Barcelona 2022
Events
We look forward to exhibiting our sensor solutions for smart home & building automation at Integrated Systems Europe 2022.
OMRON Electronic Components Europe invites you to the Integrated Systems Europe 2022 exhibition at FIRA Barcelona from 10th until 13th May 2022. Our main features at stand 2R430, hall 2 will be the latest developments in OMRON's sensor solutions for modern ventilation, lighting and access control systems.
The highlight will be on the D6T-32L Thermal Sensor with people detection algorithm for contactless measurement of the surface temperature of people and objects across 90.0° by 90.0° field of view. Live demos will be held to show how this sensor can be efficiently applied.
The D6T-32L together with OMRON Human Vision Component and B5L 3D Time-of-Flight Sensor comprises the latest technology integral for energy consumption control, but also for reliable access control, movement and occupancy monitoring, consequently facilitating COVID-19 prevention. The B5L 3D TOF is a "mechanical eye" capable of accurately and easily detecting the surrounding environment, while the HVC-P2 boasts cutting-edge facial recognition capabilities.
For ventilation systems, we will showcase the D6F-PH Pressure Sensor and 2JCIE Environmental Sensor. The exceptional accuracy at low flows of the D6F-PH and 2JCIE's versatility in measuring humidity, light level, UV, barometric pressure and air quality ensure that HVAC systems operate at optimum efficiency.
The OMRON team will be at disposal at the stand to provide all the required information and answer any questions.
When: Tuesday 10th May until Friday 13th May 2022
Where: Hall 2, stand 2R430, FIRA Barcelona Gran Via, Spain
Sensors displayed by OMRON include:

D6T-32L Thermal Sensor
The D6T-32L with people detection algorithm is a super-sensitive infrared thermal sensor that can monitor movement within a building, define occupancy ratio in an area, and control lighting and HVAC to save energy.
Applications:
- People detection modules
- Crowd density monitoring
- Gate access control
- Ventilation control

HVC-P2 Image Sensor
The Human Vision Component (HVC) with OKAO Vision is a face recognition sensor that offers ten key image sensing functions: detection of a human face, hand or body, face recognition, gender detection and estimations of age, mood, facial pose, gaze and blink. It is available with 50° and 90° FOV campera types and is easy to implement through UART or USB output.
Applications:
- Security/access control
- Digital signage
- Vending machines
- Ticketing machines
- Marketing equipment in retail

2JCIE Environment Sensor
Utilised as an IoT edge device, the 2JCIE measures noise, acceleration, eTVOC and other environmental data. It has a built-in memory and connectivity through beacon communication, and is particularly suitable for home air quality monitoring as well as earthquake detection.
Applications:
- Lighting and domotics
- Ventilation and temperature control
- Safety and security
- Smart meters

B5L 3D TOF Sensor Module
The TOF Sensor Module is a “mechanical eye” capable of accurately and easily detecting the surrounding environment even in sub-optimal conditions. Featuring a 940nm near-infrared emitter and 240 x 320 pixel receiving array, the sensor gives ranging information for the entire field of view and measures the absolute distance to objects from 0.5m to 4m.
Applications:
- Autonomous robots
- Lighting and domotics
- Security/access control

D6F-PH MEMS Differential Pressure Sensor
The digital pressure sensor is used in heat recovery units to measure air flow and detect clogged filters. Using temperature compensation, it measures differential pressure with high accuracy and repeatability over a wide temperature range.
Applications:
- Heat recovery units
- Variable air volume
- Clogged filter detection

Looking forward to welcoming you!
OMRON's expert staff will be available in hall 2, stand 2R430 to answer any questions and demonstrate the sensor solutions for smart home & building automation.