What may have caused a basic switch failure?
ID: FAQE20047E
update:
Answer
Failures of a basic switch may be caused by the following two reasons:
1. Failures related to electrical characteristics: contact failure, malfunction, contact welding, insulation degradation
2. Failures related to mechanical characteristics: operating failure, external damage
Explanation
The following electrical or mechanical characteristics failure may cause the failure of the basic switch.
![Causes and Countermeasures for Basic Switch Failure](/eu-en/sites/components.omron.com.eu/files/omron_migrate_csv/products/img/FAQE20047E-001.png)
For more information, please see "Switch Basics: Applications".
Quick tips
A relatively common cause of switch failure is deformation of the actuator lever. If the actuator lever is deformed as shown in the photo below, the switch will not work even if the actuator lever is operated, or the load for operating the switch will be too high to operate. This malfunction happened because something got caught in the lever and deformed it. As shown in the photo, when the bending angle of the lever increases or the backlash of the lever increases, the actuator lever has deformed.
![The failure case](/eu-en/sites/components.omron.com.eu/files/omron_migrate_csv/products/img/FAQE20047E-002.png)
Product category | Switches Basic Switches |
---|---|
Classification | Trouble shootings |
Related keywords |
|