What is an actuator?

ID: FAQE20010E

update:

Answer

An actuator is a component that transmits external force or movement to the internal mechanism of a basic switch. The mechanism consists of a pushbutton and lever.

Explanation

An actuator transmits external force and movement to the internal mechanism and is also useful for making the stroke longer and reducing the operating load (operating force) to make the switch easier to use. The table below shows their types.
Many different types of actuators can be attached to the actuator depending on the shape and movement of the detection object, based on a pin plunger. Select the actuator that is best suited for the shape and movement of the detection object.

Typical Actuators

For more details, see "What is a Basic Switch?" Structures.

Quick tips

Only V size switches have actuators (VAL, VAV, VAM) that can be mounted later.

Product category Switches Basic Switches
Classification Selection, Characteristics
Related keywords
  • Basic Switch
  • Actuator
  • Pushbutton
  • Pin Plunger
  • Lever
  • VAL
  • VAV
  • VAM

If the information you are looking for is not found