Can a relay be mounted in any direction?
ID: FAQE10051E
update:
Answer
Typically the mounting direction is not specified, but some models may have the mounting direction in its specification. Check the datasheet before mounting.
Explanation
Depending on the operating type and structure of the relay, some relays are easily affected by the mounting direction and others are not.
Normally, the operating characteristics in any mounting direction are within the standard range. However, for models with a large change in operating characteristics depending on the mounting direction, the direction may be specified or conditions may be added.
Refer to G7EB: Correct Use as an example.
![G7EB: Correct Use as an example](/eu-en/sites/components.omron.com.eu/files/omron_migrate_csv/products/img/FAQE10051E-001.png)
Quick tips
Make sure that there is no problem in the actual mounting direction before use.
Product category | Relays Signal Relays Power Relays |
---|---|
Classification | Usage, Applications |
Related keywords |
|