OMRON at IoT Tech Expo Global 2021
Events
OMRON will showcase solutions for smart home and building automation.
OMRON Electronic Components Europe invites you to the IoT Tech Expo Global 2021 at the Business Design Centre in London on 6th and 7th September. At stand 143 OMRON will showcase the cutting-edge sensor solutions for smart home & building automation.
OMRON has developed an extensive portfolio of components that enable intelligent control of indoor environments. The OMRON team will be at disposal at the stand to provide all the required information and answer your questions about our expanding range of sensors for ventilation, lighting and access control.
We will demonstrate how OMRON D6T-32L Thermal Sensor with people detection algorithm can reliably detect people and objects in a wide area across its 90.0° by 90.0° field of view. With its exceptional features, this sensor enables an effective infection and lighting control regime within buildings, rooms and other indoor environments.
Together with OMRON Human Vision Component and Time-of-Flight sensors, the D6T-32L creates a comprehensive state-of-the-art solution package for lighting, building access and crowd management applications.
At our stand you will also find detailed information about OMRON digital pressure and environment sensors which, combined with the D6T-32L, enhance the quality and efficiency of HVAC systems through accurate sensing of air flow, temperature, humidity and human presence.
When: Monday 6th & Tuesday 7th September 2021
Where: Stand 143, Business Design Centre, London, UK
Sensors displayed by OMRON at stand 143 include:

D6T-32L Thermal Sensor
The D6T-32L with people detection algorithm is a super-sensitive infrared thermal sensor that can monitor movement within a building, define occupancy ratio in an area, and control lighting and HVAC to save energy.
Applications:
- People detection modules
- Crowd density monitoring
- Gate access control
- Ventilation control

HVC-P2 Image Sensor
The Human Vision Component (HVC) with OKAO Vision is a face recognition sensor that offers ten key image sensing functions: detection of a human face, hand or body, face recognition, gender detection and estimations of age, mood, facial pose, gaze and blink. It is available with 50° and 90° FOV campera types and is easy to implement through UART or USB output.
Applications:
- Security/access control
- Digital signage
- Vending machines
- Ticketing machines
- Marketing equipment in retail

2JCIE Environment Sensor
Utilised as an IoT edge device, the 2JCIE measures noise, acceleration, eTVOC and other environmental data. It has a built-in memory and connectivity through beacon communication, and is particularly suitable for home air quality monitoring as well as earthquake detection.
Applications:
- Lighting and domotics
- Ventilation and temperature control
- Safety and security
- Smart meters

B5L 3D TOF Sensor Module
The TOF Sensor Module is a “mechanical eye” capable of accurately and easily detecting the surrounding environment even in sub-optimal conditions. Featuring a 940nm near-infrared emitter and 240 x 320 pixel receiving array, the sensor gives ranging information for the entire field of view and measures the absolute distance to objects from 0.5m to 4m.
Applications:
- Autonomous robots
- Lighting and domotics
- Security/access control

D6F-PH MEMS Differential Pressure Sensor
The digital pressure sensor is used in heat recovery units to measure air flow and detect clogged filters. Using temperature compensation, it measures differential pressure with high accuracy and repeatability over a wide temperature range.
Applications:
- Heat recovery units
- Variable air volume
- Clogged filter detection

Looking forward to welcoming you!
OMRON's expert staff will be available at stand 143 to answer any questions and demonstrate the sensor solutions for smart home & building automation.