Weather Sensor: Fast and Easy Way to Collect Weather Data!

WEATHER SENSOR Aratas'S Solution for Climate Sensing Applications

Our Vision

With the world experiencing ever changing weather patterns, we are recognizing increased occurrences of natural disasters and extreme weather. This along with normal needs for climate studying applications contribute to a growing need for spot weather sensing devices that are easy to install and maintain. Aratas has developed the new Weather Sensor to help solve these issues and meet these needs.

Solution Examples

Agriculture: Realize accurate climate conditions => Increase yield & reduce burden. Smart City: Forecast weather => Alert residents of sudden changes. Energy Infrastructure: Estimate supply input => Efficient power generation

Product Features

1 Easy to Install: Quick connect sensor simplifies installation in outdoor applications. 2 Easy to Maintain: Reduce the need for regular cleaning. No moving parts reduces the risk of sensors malfunctioning and breaking. 3 Low Operation Cost: Sensor operates with low power consumption at 0.8W to 1.4W (typ). RS-232C communication allows for compatibility with LPWAN protocols

Demo Dashboard

The Aratas weather sensor offers real time measurements of key climate functions temperature, humidity, barometric pressure, windspeed, wind direction, and rainfall. Below, a live demo shows our sensor readings hosted by our partner, KST Technologies.

View my Losant-powered dashboard "Aratas Weather Station Dashboard"

Weather Sensor Specifications

※ The Aratas Weather Sensor can be paired directly with the KST LoRa module for LoRaWAN connectivity.
The simple design of the sensor allows for the customer to be flexible in their design with most communication interfaces.

Video

Weathering the Challenge of Long-Range Data Communications

Weather Sensor FAQs

Q
What is the communication protocol for the weather sensor?
A
The Aratas Weather Sensor currently uses an RS232C serial communication for weather data transfer. The sensor is compatible with the KS Technologies LoRa module (KST5421-US915), and is able to function with converters onto other communication modules (such as RS485 communication). In the future, be on the lookout for additional versions that are able to work on other networks!
Q
Is Aratas able to provide the individual sensing components directly?
A
Currently, the Weather Sensor is an all-in-one component, without the possibility of using any of the sensing components individually. For additional sensing needs, however, please visit components.omron.com to learn about our other component offerings. We provide sensors for thermal IR sensing, airflow, pressure, as well as switches, connectors, and relays.
Q
What is the maintenance protocol for the weather sensor?
A
The Aratas Weather Sensor is a solid state solution, including all sensors contained in a singular housing. The sleek design of the sensor is designed with minimal maintenance in mind, so there is less need for regular checks on equipment. The sensor also uses optical and ultrasonic sensors for rain and wind, eliminating moving parts in the sensor design.
Q
Is the Weather Sensor able to transfer data in remote areas?
A
Yes, low power capabilities of the sensor allow for the device to work with most long distance and communication protocols. Aratas’s small data transfer package allows capability of working with several different communication methods that can cover a wide range for data transfer.
Q
Can I power this weather sensor with a solar panel setup?
A
Yes, the low power requirements of the Aratas Weather Sensor allow it to function powered by most conventional solar panel setups.
Q
What is the refresh rate for the weather sensor?
A
Data is sent through the Weather Sensor each minute.
Q
I don’t have much experience with weather sensors, is there a way I can get some help?
A
Our team is available to help you with your setup and any information you need to get your project up and running. Our engineers have a lot of experience with different applications using the weather sensor, and we are able to work with you to ensure you have the best possible installation for the start of your project.

Contact Us

Related Contents

IoT Breakthrough Award 2026

Aratas Named Winner of 2026 IoT Breakthrough Award