Compact PCB relays instead of contactors | Advantages and practical examples of replacing PCB relays will be presented!(Large current,High voltage)Ask Aratas Now

Do you have any of the following concerns?

We want to make our products more competitive by focusing on cost performance! But how can we lower the cost any further…
We want to develop smaller and slimmer products! We are using a contactor with screw mounts, but is there any way we can make it into a circuit board ?

As customers’ products become higher capacity, contactors, which are suitable for controlling large power, are utilized as load switching devices for various electrical equipment requiring large current and high voltage. With the growing need for smaller, lighter and thinner equipment, however, there is an increasing trend to consider replacing large-sized contactors with PCB relays (printed circuit board relays) that are smaller in size and have higher capacity to interrupt large currents and voltages.
In addition, some of our customers are also reducing costs by using PCB relays to integrate load switching devices into a board as one way to reduce man-hours during production, in anticipation of a future surge in demand and expansion of production volume.

Growing needs /  Smaller, lighter, and thinner / Assembly man-hour reduction (cost reduction)

As the replacement of contactors with PCB relays progresses in this way, customers may face psychological hurdles to replacement because of the significant design change from conventional cabling and wiring to “integration into PCB”.

In this article, we will introduce various replacement advantages, points to note, actual replacement examples, and our approach to what are the key points for designing PCB relay mounting boards?, which can be provided only because Aratas owns both contactors and high-capacity PCB relays.

Evolution of PCB relays and increasing capacity

 

In the past, contactors have been utilized to control large currents, such as those exceeding 30 A, while PCB relays have been utilized to control currents below 30 A. With advances in technology, however, thick copper substrates capable of withstanding large currents and compact PCB relays (PCB relays) capable of turning on and off large currents and voltages are appearing one after another.

As a result, some of the area bands that were conventionally controlled by contactors can now also be controlled by PCB relays. For example, Aratas’s PCB relays can cover current and voltage ranges up to 1000 VAC/VDC and 300 A.

Visual comparison between a traditional bulky contactor and a compact Aratas high-capacity PCB relay.

Example of Replacing Contactors with High-Capacity PCB Relays

 
Voice of Customer

Replacement study example (1): Circuit-boarding realizes low-profile design

 
Voice of Customer

Designer
EMS Division, DAIHEN Corporation

In developing the industry's first unit-type power conditioner (170 kW) compatible with high voltage (1500 VDC), which was released in 2024, the challenges I faced were to make the equipment smaller and to increase the voltage.
In order to reduce the size of the equipment, I proceeded with replacing large contactors with PCB relays. In my search for PCB relays with 1000 VAC withstand voltage and high capacity to achieve higher voltages, I consulted with Aratas, who at the time had the only PCB relay lineup in the relevant capacity range.
Although I had the idea of making a circuit board, I often struggled as it was my first attempt.
However, Aratas not only provided me with suggestions regarding relays, but also introduced me to a circuit board manufacturer and provided me with a lot of support in terms of circuit board mounting design, which enabled me to successfully reduce the size and increase the voltage of the power conditioner. I am particularly impressed with the effect of the replacement of contactors with PCB relays, which has reduced the height of the equipment to less than half.
Our development of the unit-type power conditioner makes it possible to continue operation by isolating only the faulty parts, thereby reducing downtime on site. Furthermore, by changing the number of units, the conditioner can also be used for private consumption in factories, allowing us to broaden the scope of our proposals.
Having heard that Aratas will continue to expand its lineup of large-current, high-voltage PCB relays, I have high expectations for Aratas and look forward to their continued cooperation.

Diagram showing the space-saving benefits on a control board by switching to PCB-mounted relays.

DAIHEN's unit-type power conditioner

Calculation chart comparing the power consumption of contactor coils vs. Aratas power relays.

DAIHEN's unit section

Diagram showing the space-saving benefits on a control board by switching to PCB-mounted relays.

DAIHEN's unit-type power conditioner

Calculation chart comparing the power consumption of contactor coils vs. Aratas power relays.

(Overhead view from above)

 

Replacement study example (2): Circuit-boarding halves the number of man-hours required to assemble a single unit!

 
Thermal image showing reduced heat generation in relay-based designs compared to contactors.

Aratas salesperson (Japan)

As a cost reduction measure, there are an increasing number of cases where the replacement of contactors with PCB relays is being considered in fast chargers.
For systems that require multiple units to be controlled, the number of contactors used will increase, and in some cases more than 100 contactors may be required on a single quick charger. 
In such cases, assembly requires a lot of man-hours and manpower, including contactor screw installation, busbar screw installation, crimp terminal press-fitting and wiring, and finally, inspection of each individual item, resulting in the assembly of a single quick charger requiring many hours of work. 
However, I have heard from our customers that the man-hours required for cable wiring, screw tightening, etc. can be reduced by half by making a circuit board and replacing contactors with PCB relays.
Since the replacement is also expected to have the effect of reducing material costs, I would like to proactively propose the replacement.

 

Replacement study example (3): Circuit-boarding is being adopted in Europe ahead of other regions

 
Thermal image showing reduced heat generation in relay-based designs compared to contactors.

Aratas salesperson (Europe)

In Europe, the trend of developing PCB based instead of panel and DIN rail mounting solutions is already well established avoiding manual mounting and wiring labor costs. Designers have shared their frustration when attempting to value engineer or develop new Inverter related products that needs further space and energy saving.
PCB lends itself especially well to achieving design flexibility. It also affords more opportunity to make reduction to heat dissipation which in turn can result in indirect cost savings and extended electrical life. I’ve helped customers achieve improved solutions in Solar PV Inverters, wall and pedestal mounted EV Chargers, Energy Storage Systems and UPS and more recently in building and factory automation where I’m actively proposing our relays.

Difference between contactors and PCB relays

 
Contactor Compared to PCB relays: High switching capacity,Larger size Higher power consumption Mainly screw-tightened Slow response time,Available in harsh environments
PCB relay Compared to contactors: Small switching capacity Compact & lightweight Low power consumption Limited operation environment PCB terminal

What is a contactor?

Example of a high-power switching PCB design for EV chargers using Aratas G7EB relays.

Contactors are applied to large installations, e.g., starters for electric vehicles, large lighting control systems. They are also called electromagnetic contactors. Compared to relays, they are designed to control higher currents and voltages and are more robust. As a result, they tend to be larger in physical size and weight than relays, and their switching speeds tend to be relatively slow. In addition, since the electromagnetic coil is large in proportion to the open/close capacity, power consumption tends to be large. The most common installation method is screw-tightening.

What is a PCB relay?

Application of Aratas G9KA relays in PV inverters to improve power efficiency and reduce size.

In general, PCB relays are applied to smaller capacity equipment compared to contactors. Although less robust than contactors, they are now possible to energize, open, and close even loads as large as 300 A by optimizing the magnetic flux design, contact point shape, and arc interrupting path, and utilizing CAE analysis. Compared to contactors, they are smaller, lighter, and can be driven with lower power consumption. The terminal shape is designed to match the board and peripheral components (e.g., terminal block) for printed circuit board terminals (PCB terminals).
(Example of our products: G9KA, G9KB, G9KC)

What are the advantages when replacing contactors with high-capacity PCB relays?

 
Merit01

Realization of space-saving design

 

The major advantage of high-capacity PCB relays is that they are mounted directly on the PCB, making them more compact than contactors when wiring space is factored in. For example, in energy-related equipment, space-saving component mounting can reduce overall equipment size and simplify wiring. They also contribute to effective use of limited installation space.

Example: Comparison of mounting when replacing a contactor with a PCB relay with 3a contacts

Height Approx. 140 mm

55 mm

Reduced by 61%
Volume 2,940,000 mm3

425,000 mm3

Reduced by 85%
Weight Approx. 2.5 kg/pc

Total of 0.7 kg/3 pcs

Reduced by 72%

Note: Comparison between a typical contactor in the 200 A band and the relay board module we assume (based on our own research, January 2025).

Merit02

Cost reduction and higher mass production efficiency

 

Contactors, which are mostly screw-mounted, are difficult to automate mounting and wiring, and manual work is time-consuming and costly.
In contrast, relays for printed circuit boards (PCB relays) can be easily installed with automated equipment such as pick-and-place machines and flow soldering machines. Therefore, they are easy to integrate into automated manufacturing processes and can significantly reduce manufacturing costs as production volumes increase.

Example: Cost comparison when applied to a PV power conditioner Contactor(When used with two 3a contacts in series) VS Relay PCB module(When used with three sets of two 1a contacts in series)

Cost of interconnected system’s load switchgear Reduced by approx…35% Cost comparison with 200 A band load switching control unit When using contactors (with busbar and screw) When using PCB relays (with PCB and terminal block)<= Not only the cost of load control components, but also the cost of assembly, such as screw tightening and wiring, can be reduced by about half!

* Cost comparison of a control unit when replacing 2 contactors (3a, 200 A) x 2 with 6 relays (1a, 200 A). Our simulation results (as of January 2025)
These are simulation results under specific conditions and effectiveness is not guaranteed.

Technical data showing the arc-extinguishing performance of Aratas DC power relays.

Safety features equivalent to contactors

 

Many high-capacity PCB relays have the weld detection function (optional auxiliary contact with mirror contact structure conforming to IEC60947-4-1) required of contactors and improved insulation resistance. As with contactors, they contribute to a high level of safety.
There are also models with high short-circuit current withstanding capacity in compliance with IEC62955, the standard for EV chargers, and models that guarantee insulation performance with a contact gap of 3.6 mm or more in compliance with VDE0126, the solar power generation standard.
As some of these products ensure reliability in short-circuit and high-voltage environments, they can be reliably used in energy-related equipment.

Guide to creepage and clearance distances for high-voltage PCB relay applications.

In a combination of a relay body and an auxiliary contact block, if the a-contact (main contact) of the relay body is welded, all b-contacts of the auxiliary contact block are ensured a minimum withstand voltage of 2.5 kV or a minimum contact gap of 0.5 mm even after the coil is de-excited.

Image of mirror contact structure

Reliability metrics for Aratas PCB relays in high-frequency switching and harsh environments.

Improved connection reliability

 

Since contactors are manually screw-tightened, although the fastening torque, such as the screw tightening method and tightening strength, is determined, there are cases where variations in fastening force are inevitably caused by different workers. By using PCB relays instead of contactors, the number of screws can be greatly reduced, contributing to improved connection reliability.

Example: Comparison of the number of screws when applied to a PV power conditioner Contactor(When used with two 3a contacts in series) Number of screws 20 / Relay PCB module (When used with three sets of two 1a contacts in series) Number of screws 10 Approx. half of contactor

What should you be aware of when replacing contactors with high-capacity PCB relays?

 
Infographic showing the environmental impact reduction and energy savings when switching from contactors to PCB relays.

Limitation of maximum current and voltage capacity

 

Nowadays, PCB relays are becoming high-capacity and replacing contactors in the mainstream high-power area at an alarming rate. However, the maximum current that PCB relays can hold is lower than that of contactors in the high capacitance range, due to the copper foil thickness of the board and the limitation of the current value that can flow on the board. (In the case of our relays, they are currently capable of handling up to 1000 VAC/VDC and 300 A level loads as of October 2024). Contactors may be better suited for applications that control very large currents, such as large industrial equipment or three-phase motors, necessitating selection based on load requirements.

Cost-benefit analysis chart comparing the lifecycle costs of contactors versus Aratas power relays.

We are adding PCB relays that can control even higher current and voltage loads to our lineup.

We can help you with any PCB relay problems! Please feel free to contact us with any requests regarding PCB relay specifications. Ask Aratas Now

Diagram illustrating the reduction in total equipment weight achieved by using PCB-mounted power relays.

Additional heat-dissipating structure

 

A barrier to downsizing and higher capacity is the heat generated in the equipment. For example, if the current-carrying capacity of a PCB relay is doubled due to higher capacitance, the amount of heat generated will quadruple. If the temperature becomes too high, however, the board will be damaged. Therefore, PCB relays that carry large currents in the 200 - 300 A class require heat dissipation structures such as fans and heat sinks on the board in some cases. Please consider appropriate cooling and heat dissipation measures as needed.

Aratas also offers a lineup of high-capacity PCB relays with low contact resistance (e.g., initially 0.2 mΩ or less in G9KA), contributing to smaller and thinner devices by reducing heat generation inside devices and heat dissipation mechanisms.

Fan Heat sink
Caution03

Maintainability

 

PCB relays are mounted on the board by soldering, making pinpoint component replacement difficult in the event of failure. In many cases, the entire circuit board is replaced.
You might think that replacing the entire circuit board would be more expensive than replacing only the faulty component. However, since the entire board is new, it can be replaced in a single replacement without the need to send workers to the site to identify the faulty component. The time required for replacement work can be reduced, resulting in improved equipment uptime.

By replacing the entire board, Maintenance man-hour reduced, Equipment downtime reduced
Caution04

Vibration resistance

 

The contactor has a highly robust structure that increases contact pressure and is resistant to vibration. For this reason, contactors are often used in automotive and other applications. Their proven track record has been recognized and utilized in other applications with high vibration characteristics. High-capacity PCB relays can also be made more vibration-resistant by devising contact shapes, etc. If you have any requests, please feel free to contact us.

What are the key points for designing PCB relay mounting boards?

 

When considering integration onto a circuit board, you may be asking yourself, “What kind of components are needed?”, “Is it okay to energize the board with a large current?” and so on. Please refer to the following articles for design tips.

Point01

Example of peripheral components required for high current control system utilizing PCB relays

 

The following is an example of required components for a relay PCB module (when used with three sets of two 1a contacts in series). A component such as a thick copper board capable of carrying a large current is required.

Component Pieces
Relay (SPST-NO (1a))
* Less in number of components in case of multi-pole relay
6
Printed circuit board 
(thick copper board)
1
Busbar 6
Terminal block 6
Screw 4
Case study visual: Comparison of internal control panel space before and after replacing contactors with relays.
Point02

PCB design, mounting conditions

 

●Board design conditions considering heat generation and dissipation

In addition to high-density mounting on a board, it is important to adopt a board that fits the component layout and conditions if you want to energize the device with a large current. In general, the design should take into account the appropriate board thickness, copper foil cross-sectional area, terminal block size, and distance between main terminals for the rated current of each relay. For detailed condition examples, please refer to the link on the right.

●Mounting conditions for printed circuit board terminals

To keep the terminals from rising in temperature and overheating, high-capacity PCB relays may require terminals with a large surface area. For the concept and recommended profile of how to solder mount on the board, please refer to the link on the right .

Point03

Heat measures

 

It is also important to minimize heat dissipation mechanisms such as fans and heat sinks by controlling the heat generated by the components themselves. Relays are sometimes regarded as components that generate heat relatively easily, but heat generation can be controlled by selecting relays with low contact resistance.

Our relays feature “low contact resistance and low heat generation”. We also offer a product (G9KA) that is capable of maintaining an initial value of less than 0.2 mΩ, which is equivalent to a contactor, and less than 0.3 mΩ after electrical durability. Simulation results show that replacing a conventional general high-capacity relay with our relay reduces the initial resistance by 0.2 mΩ, resulting in a temperature rise of approximately 19.3°C (G9KA) and 67.7°C (G9KA-E). Please consider this. (For details, click here)

Point04

Low power consumption by holding voltage circuit

 

It is recommended that high-capacity PCB relays be controlled by “holding voltage circuit” or “PWM drive circuit” to minimize power consumption. Depending on the circuit, it is theoretically possible to reduce the drive power to 1/4. For circuit examples, please refer to the links on the right or the white papers on each product page.

Aratas’s high-capacity mechanical relay lineup

 

Aratas’s high-capacity PCB power relays offer a product lineup suitable for a wide range of applications from low to high voltages. Select the optimum relay for your design.
Please feel free to contact us if you need help in selecting the right one.

 

We can help you with any PCB relay problems! Please feel free to contact us with any requests regarding PCB relay specifications. Ask Aratas Now

Related contents

 

High Capacity Relay Technical Support Page

A technical support page for high-capacity relays that provides detailed explanations of “questions” when using PCB power relays with large current and high voltage, such as reverse voltage of coils, holding voltage application circuits, recommended conditions for large-current PCB flow soldering, effects of magnetic fields, and precautions when connecting in series or parallel.

Global safety standard compliance map (UL/IEC) for Aratas high-capacity power relays used in power switching.

Energy Market Solutions

Aratas will introduce the solutions that we provide to customers for related equipment from energy generation to utilization, categorized into “Commercial/Industrial” and “Household” applications.

Graphic showing Aratas's reliability testing standards for high-voltage DC and AC power switching components.