MEMS Flow Sensors Features


Realizing a highly accurate flow measurement, sensing even a single flap of a butterfly’s wings
Omron’s MEMS flow sensor accurately detects minute airflow so much as a single flap of a butterfly’s wings.
A gas flow sensor capable of “measuring mass flow” independent of temperature and pressure.



Mass Flow Measurement
Q1 | There are two balloons; each having different volumes. But these balloons have the same mass. Why is that? |
A
|
The volume increases/decreases according to the pressure and temperature changes. The mass, on the other hand, remains constant regardless of the environmental changes. The mass flow measurement allows measurement performance that is not affected by the changes in the environment. |
Q1 | Why is mass flow measurement required? |
A
|
An accurate measurement of the flow is required especially for combustion control. Omron’s flow sensor enables measuring the gas flow based on the mass flow measurement. |
Principles of MEMS Flow Sensor Measurement
D6F Series

During the absence of airflow, the temperature distribution around the heater is symmetrical. When there is airflow, the temperature of the upwind side cools down and the temperature of the downwind side warms up, disrupting the symmetry of the temperature distribution.

By detecting this temperature difference appearing as a difference in the electromotive forces developed by the thermopiles, it allows the mass flow rate and mass flow velocity to be measured without the influence of temperature and pressure. Since the thermopile generates the thermo-electromotive force, the power consumption is much lower than when using the resistivity method.
MEMS Air & Gas Flow Sensors are Highly Resistant to Dust
Built-in Dust Segregation System (cyclonic)
The sensor can be placed anywhere thanks to its dust-resistant structure. Omron’s unique design of 3D flow path provides a high level of reliability by separating dust particles to reduce its effect on the sensor chip. Additionally, Omron succeeded in reducing the sensor size, allowing it to be used in wider range of applications.


solutions-lineup-sensor
MEMS Flow Sensors Selection MEMS flow sensors can be searched by various specifications
Light Convergent Reflective Sensors – Application Guide View a collection of use cases of limited reflective sensors, issues and improvements
Environmental Sensors Introducing the features, lineup, and applications of environmental sensors
Photomicro Sensor Selection Choose from a wide range of variations of photomicro sensors to suit your application
OMRON's Touchless Sensors Lineup Introducing OMRON’s touchless sensors at a glance
What is IOT? The role of advanced IoT sensors is explained
OMRON's MEMS Sensors Introducing OMRON's MEMS products, technologies, and application examples
Light Convergent Reflective Sensor A reflective sensor that accurately detects the presence or absence of an object within a limited range