DA POWER RELAY G7L G7L-2A-BUBJ AC100/120 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ AC200/240 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ DC6 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ DC12 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ DC24 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ DC48 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ DC100 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-B-CB AC24 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUB AC50 RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUB AC50 BY OMI RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BJ-CB AC200/240 BY OMI RoHS compliant Login/Register
DA POWER RELAY G7L G7L-2A-BUBJ-CB DC110 BY OMI RoHS compliant Login/Register

Management Criteria for Regulated Chemicals

For issuance of our “Certificate for Non-inclusion of Chemical Substances in Products/Materials”, the following criteria apply to prohibited chemicals.

Management Criteria for Regulated Chemicals (Ver. 5.00) <PDF 0.5MB>

Views on California Proposition 65

We will explain how the products handled by OMRON Device & Module Solutions Company (excluding excluding industrial-purpose products) comply with California Proposition 65.

Removal of the Ro Mark placed to individual packaging boxes and packaging labels of Omron products

At Omron, we previously placed the Ro Mark (*1) to individual packaging boxes and packaging labels of our products. The mark was used for the internal operation to identify use/non-use of specific chemical substances based on internal criteria. This internal operation to use the Ro Mark will end in March 2025.
Accompanying this change, the Ro Mark will be removed from individual packaging boxes and packaging labels successively.
The Ro Mark was used for internal identification purpose and it was not used to guarantee use/non-use of certain chemical substances to customers.  
To confirm use/non-use of RoHS designated chemical substances, please download the Certificate of Non-inclusion from this website.

Ro
*1: Ro Mark

Discontinuation of the Ro mark to product packaging of Omron products<PDF 0.18MB>

  • *1: Compliance status
    • "RoHS compliant" in the datasheet indicates that products of this product model do not contain any of the 10 chemicals restricted under EU RoHS.

    "RoHS compliant" indicates that Omron can deliver RoHS-compliant products for this model, and does no necessarily mean that all the products of this model are compliant with RoHS.
    Some existing stock products may not be RoHS-compliant depending on the purchase date.

    *EU RoHS Directive: (ten restricted substances and their respective maximum levels:
    Lead (Pb) : 1,000 ppm, Mercury (Hg): 1,000 ppm, Cadmium (Cd) : 100 ppm, Hexavalent chromium (Cr(VI)) : 1,000 ppm, Polybrominated biphenyls (PBB) : 1,000 ppm, Polybrominated diphenyl ether (PBDE) : 1,000 ppm, Bis(2-ethylhexyl) phthalate (DEHP or DOP) : 1,000 ppm, Butyl benzyl phthalate (BBP) : 1,000 ppm, Dibutyl phthalate (DBP) : 1,000 ppm, and Diisobutyl phthalate (DIBP) : 1,000 ppm The above restrictions do not apply to items exempted by the RoHS Directive. We have confirmed that the four phthalates are not intentionally used in our products over the threshold value.

  • *2 Downloading of Certificate of Non-inclusion
    • You can download Certificate of Non-inclusion which certifies that the product does not contain chemical substances/substance groups restricted by Omron.

Search by product type

*Please contact us or distributors for products that are not found on e-web.