Environmental Sensors
Integrating various sensing
capabilities into
one single IoT sensor
Environmental Sensors
Omron’s Environmental Sensors is a multi-function sensing component capable of tracking eight different environmental factors which include: temperature, humidity, light, UV index, barometric pressure, noise, acceleration and VOC (Volatile Organic Compounds) with wireless communication functionality in an ultra-small footprint.
Combines Bluetooth® low energy technology with different sensing capabilities. Immediately available for your use.
Multiple sensing capabilities in one package. Users can choose different locations to sense the surrounding environment.
All sensing data is stored in the internal memory of the device. Users can access it at all times without having to worry about loss of data.
Sensor functions
Temperature
Humidity
Light
UV Index
Barometric Pressure
Noise
Acceleration
VOC
Environmental Sensors Product Lineup
Choose from three types of sensors based on your needs.
Applications & Uses for Environmental Sensors

- Monitoring living spaces
- Family safety


- Heatstroke prevention
- For a good night’s sleep

Temperature
Humidity
Light
Barometric Pressure
Noise
Acceleration
VOC

- Detection of changes in weather conditions


- Heatstroke and UV intensity alert

Temperature
Humidity
UV Index
Barometric Pressure
Noise

- Monitoring office environment
- Maintaining comfortable workplace environment

Temperature
Humidity
Light
Barometric Pressure
Noise
Acceleration
VOC

- Maintaining the quality of factory environment

Temperature
Humidity
Light
Barometric Pressure
Noise
Acceleration
VOC
Concept for Environmental Sensors
For greater Simplicity in Connectivity and Sensing in IoT

-
Sensor beacon mode allows sending of data to IoT gateway devices
- Beacon transmits environmental data (broadcasting).
- Users can configure their own applications.
-
Cloud collaboration accessible on smartphones
- The amount of data captured on smartphones can be stored in the cloud.
- Environmental data can be checked from smartphones in remote locations.
Bluetooth® Environmental Sensors Specifications
Model | Appearance | Communication interface | Output data | Minimum packing unit (Unit: pcs) |
---|---|---|---|---|
2JCIE-BU01 | ![]() |
Bluetooth®∗1 low energy, USB communication |
Temperature, Humidity, Light, Barometric pressure, Sound noise, 3-axis acceleration∗2, eTVOC∗3, Discomfort index∗4, Heat stroke warning level∗4, Vibration information∗2 (No. of earthquakes, No. of vibrations, SI value∗5) | 1 |
2JCIE-BL01 | ![]() |
Bluetooth®∗1 low energy | Temperature, Humidity, Light, UV index∗6, Barometric pressure, Sound noise, Discomfort index∗4, Heat stroke warning level∗4 | 1 |
2JCIE-BL01-P1 | ![]() |
Bluetooth®∗1 low energy | Temperature, Humidity, Light, UV index∗6, Barometric pressure, Sound noise, Discomfort index∗4, Heat stroke warning level∗4 | 1 |
- ∗1. The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc. and any use of such marks by OMRON Corporation is under license.
- ∗2. 3-axis acceleration values can only be obtained in the specified operation mode. For details, refer to the Communication Interface Manual.
- ∗3. eTVOC (equivalent Total Volatile Organic Compounds) refers to the total concentration of volatile organic compounds in a room environment. Output TVOC values will be higher or lower depending on the type of volatile organic compound. Also, if continuously operated in high-temperature and high-humidity environments, sensitivity for eTVOC values may decrease.
- ∗4. Information for heat stroke and discomfort index are only guidelines to be used for air conditioning and physical condition management. An individual difference and physical condition will greatly affect an individual feeling. Sensor output is not to be used for determining the presence of symptoms. Use only as a guideline. Warning levels for heat stroke may not be the same as those issued by public institutions.
- ∗5. SI (Spectral Intensity) values corresponds to the destructive energy seismic motions exert on a structure.
- ∗6. Information on UV Index is just for reference. And it may not be the same as that issued by public institutions.