What are corrosion-resistant basic switches?

ID: FAQE20013E

update:

Answer

There are various types of corrosion and Aratas’s basic switches have various specifications such as gold contacts, sealed structures, and built-in reed switches that will help prevent corrosion. Select proper specification as needed.

Explanation

Oxidation and sulfurization of silver contacts are inevitable due to the external environment. However, it is possible to reduce the influence by using gold contacts, sealed structures, and built-in reed switches.
The criteria for the environment cannot be defined. It is recommended to perform evaluation under actual usage with the following types of switches:

  • Those that use gold contacts (0.1A rating or microload switching compatible product)
  • Sealed basic switch (less susceptible to external environmental influences because its structure prevents water from entering)
  • Built-in reed switch type (D2RV)

Note that the metal parts other than contacts are affected.

For more information, see "Basic switch” Structures.

Quick tips

No Tips

Product category Switches Basic Switches
Classification Selection, Characteristics
Related keywords
  • Basic Switch
  • Gold Contact
  • Silver Contact
  • IP67
  • Oxidation
  • Sulfidation
  • Buit-in Reed Switch

If the information you are looking for is not found