What sensors are suitable for measuring distance?

ID: FAQE40055E

update:

Answer

Our lineup includes multiple sensor products that enable distance measurement.
Please refer to the features and application examples of each product to assist you in solving challenges and selecting the right product.

① 3D TOF Sensor Module (B5L)
② Micro Displacement Sensor (Z4D)

Explanation

① 3D TOF Sensor Module (B5L)

This sensor module uses the TOF (Time Of Flight) method to measure the distance to people within the 3D area based on the flight time of light.

Achievement

■Application: Service robot

This sensor module can be installed in a service robot to measure the distance to an object within the 3D area, enabling the host side to perform control actions such as deceleration and stopping based on the measured distance.

② Micro Displacement Sensor (Z4D)

This displacement sensor uses triangulation for high resolution of ±10μm. It is minimally affected by the reflectivity of detected objects, such as their color.

Achievement

■Application: Bill changers

This sensor can measure the distance from the sensor to the bill with a high resolution of ±10µm and detect two bills inserted at a time.


Product category Sensors Displacement Sensors/Ranging Sensors 3D TOF Sensors Module Micro-displacement Sensors
Classification Trouble shootings

If the information you are looking for is not found