After delivery, some Photomicrosensors do not work. Please advise possible causes and countermeasures.

ID: FAQE40028E

update:

Answer

One of the causes is estimated to be a decrease in light current due to aging of the Photomicrosensors LED. In this case, the circuit design should be reviewed.

Explanation

LED elements have the characteristic that the light emission output gradually decreases over time. Because the Photomicrosensors use a non-contact detection method, they have higher reliability than mechanical switches and are effective in extending the life of equipment. However, it is based on a circuit design that takes into account the aging of the LED. By setting a threshold with sufficient margin, stable detection over a long period of time can be performed on the equipment.
For details, refer to Thecnical Information for Photomicrosensors as well as the following related FAQ.

Quick tips

No Tips

Product category Sensors Photomicro Sensors
Classification Trouble shootings
Related keywords
  • Optical Sensor
  • Trouble Shoting
  • Products Which Can Not Detect
  • LED Degradation
  • Light-Emitting Power
  • Ligjt Current
  • Life-Time Extension?
  • Stable Sensing

If the information you are looking for is not found