What is the heat-resistant temperature for a relay when manually soldering, and what are the precautions for manual soldering?
ID: FAQE10059E
update:
Answer
Please refer to Explanation about manual soladering for our relays.
Explanation
- After smoothing the iron tip, solder according to the following conditions:
- Soldering iron: 30 to 60 W
- Iron tip temperature: 350°C
- Soldering time: Within about 3 seconds
- Use non-corrosive rosin for the flux because of the compatibility with the relay components.
Use an alcohol solvent with less chemical action for flux. - When soldering the terminals, make sure that no solder, flux, or solvent adheres to any part other than the terminals. If solder, flux, and/or solvent enters the inside, it could cause insulation degradation and poor contact.
For more information, see Safty Precautions for All Relays: 6-10 Automatic Mounting of Relays for PCBs.
Quick tips
Note that, as shown in the figure below, some solders have a cut surface to prevent flux from scattering.

We have prepared a technical support page dedicated to high-capacity relays that explains in detail "I don't know" when using high-current, high-voltage PCB power relays, such as back EMF voltage (Zener diode and varistor) of the coil, holding voltage application circuit, recommended conditions for high-current substrate flow solder, the influence of magnetic fields, and precautions when connecting in series and parallel. Please also use this as well.
Click here for the high-capacity power relay technical support page.
Product category | Relays Signal Relays Power Relays |
---|---|
Classification | Mounting, Storage |
Related keywords |
|