What is the sealing performance (waterproof, dustproof, gas resistance) of a basic switch?

ID: FAQE20030E

update:

Answer

Omron basic switches have a lineup of IP40 to IP67 protective structures with waterproof and dustproof specifications conforming to the protective structure. We have sealed basic switches with IP67. Please note that we do not have standards for gas resistance.

Explanation

For some models we can provide test data for reference only. Accelerated test data cannot evaluate how many equivalent years correspond in the actual environment.
Do not use the product in an atmosphere with high temperature and humidity or in a harmful gas such as sulfide gas (H2S, SO2), ammonia gas (NH3), nitric acid gas (HNO3) or chlorine gas (Cl2). It may cause malfunction such as contact failure or damage due to corrosion.

Quick tips

No Tips

Product category Switches Basic Switches
Classification Usage, Applications
Related keywords
  • Basic Switch
  • Sealed Basic Swich
  • Protective Structure
  • IP40 IP67
  • Water Resistance
  • Dust Resistance
  • Gas Resistance

If the information you are looking for is not found