What is an actuator?
ID: FAQE20010E
update:
Answer
An actuator is a component that transmits external force or movement to the internal mechanism of a basic switch. The mechanism consists of a pushbutton and lever.
Explanation
An actuator transmits external force and movement to the internal mechanism and is also useful for making the stroke longer and reducing the operating load (operating force) to make the switch easier to use. The table below shows their types.
Many different types of actuators can be attached to the actuator depending on the shape and movement of the detection object, based on a pin plunger. Select the actuator that is best suited for the shape and movement of the detection object.

For more details, see "What is a Basic Switch?" Structures.
Quick tips
Only V size switches have actuators (VAL, VAV, VAM) that can be mounted later.
Product category | Switches Basic Switches |
---|---|
Classification | Selection, Characteristics |
Related keywords |
|