What are soldering methods and conditions for a basic switch?
ID: FAQE20038E
update:
Answer
In addition to the basic soldering method of basic switches (see Explanation), note the following:
・Soldering operation should be performed at or below the temperature and time specified in the specifications, and external force should not be applied for 1 minute after soldering.
・Pay attention to the insulation distance after soldering.
・When soldering to PWB, apply flux inhibitor (such as Surflon) to the switch mounting surface before use.
・Do not clean open type switches after soldering.
Explanation
The basic soldering method of basic switches is shown below.
Quick tips
No Tips
| Product category | Switches Basic Switches |
|---|---|
| Classification | Mounting, Storage |
| Related keywords |
|