How many pieces are in a package for basic switches?

ID: FAQE20039E

update:

Answer

The number of pieces in a unit packaging (smallest package) is as follows:
・V size: 100 pieces
・S size: 500 pieces
・J size: The number of pieces in a package varies depending on a model.

Explanation

The V size is based on the NECA4505 V type, and the size of the box depends on whether it is the button type or lever type.
However, the lever type comes in several box sizes depending on the length of the lever. The V size is packed in a box aligned on a tray, while some types of S and J size are packed in nylon bags instead of being aligned on a tray.

Quick tips

The packaging box is designed with consideration for the vibration and impact during transportation. We recommend that you order based on the minimum number of pieces in a package.

Product category Switches Basic Switches
Classification Mounting, Storage
Related keywords
  • Basic Switch
  • Unit Packaging
  • Packed in a Box
  • Vibration Impact During
  • Transportation
  • Minimum Packaging Unit

If the information you are looking for is not found