×
Our web site is compatible to the following browsers:Chrome (Latest),Edge (Latest),Firefox (Latest),Safari 9+,Internet Explorer 9 (Limited),Internet,Explorer 10 (Limited), Internet Explorer 11
Please update your browser for your better access
Sound recording cannot be done. Only acoustic pressure (noise) can be measured.
Can I export the product?
This product emits radio waves and may require authentication depending on a country or region.
For details, please inquire through our contact form.
Is it RoHS compliant?
Yes.
Can Omron calibrate the product?
No, we do not provide a calibration service.
What kind of guidelines do you use for calculation of heatstroke alert level?
It is based on the heat index WBGT(Wet Bulb Globe Temperature).
WBGT is recognized as one of the effective guidelines for working and exercise environments, and is internationally standardized by ISO and other organizations.
BAG Type Environmental Sensor - 2JCIE-BL01
Can I change the measurement interval?
Data output can be set in seconds between 1 to 3600 seconds.
Can I log the sensing data?
The built-in flash memory can log 26,624 measurement data and can be read out any number of times.
If the memory becomes full, data is overwritten from the oldest one.
I put in the battery but the LED does not light up. Is it damaged?
The LED turns off in a short time.
Please check the front window of the Environmental Sensors immediately after setting the battery to the electrode.
The time period for the LED to light up is about one second.
Is it possible to get measured data simply by receiving BLE's Advertise?
By changing to Broadcaster Mode, data can be included in Advertise and sent.
How do I change to Broadcaster Mode?
You can change Beacon Mode (UUID: 0x0C4C3042...) with a generic Bluetooth®∗ low energy application.
Please refer to section 2.4.2 of the user's manual for the value to write.
∗ The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc. and any use of such marks by OMRON Corporation is under license.
How do I retrieve measured data?
You can use the setup screen of the smartphone application "Environmental Sensors" to perform CSV output.
Can I reset data on flash memory?
No, there is no reset function on the flash memory.
USB Type Environmental Sensor - 2JCIE-BU01
Can I change the measurement interval?
The measurement interval is fixed to one second.
Can I log the sensing data?
The built-in flash memory can log 60,000 measurement data and can be read out any number of times. If the memory becomes full, data are overwritten from the oldest one.
Can I change the log interval to flash memory?
Data output can be set in seconds between 1 to 3600 seconds.
The output contains CO2. Does it have a CO2 sensor?
No. The eCO2 (equivalent CO2) value is an equivalent value of carbon dioxide concentration calculated from TVOC value. It cannot directly detect CO2 concentration.
Can the power be supplied from devices other than a computer?
The power can be supplied from a USB port of an AC adapter or a smart tap.
Does measurement start when power is supplied?
When power is supplied, measurement and transmission of Advertise will start. Note that measurement data is saved in the flash memory after the time information is written.
Can I reset data on flash memory?
You can erase data saved on flash memory using the Memory reset function.