EE-SX3173/4173-P Photomicrosensor (Transmissive)
Built-in Photomicrosensor
Connector Type
- Mounted with M3 screws
- 5 VDC and 24 VDC power supply types are available
- Photo IC output (Dark-ON/Light-ON)
- Connector with secure lock compatible with JST GHR-03
- Equipped with a Zener diode, which increases noise immunity
(for EE-SX3173/4173-P3-Z only) - Connector with cable is also available (order separately)
EE-5002 1M
- English
Datasheet
- English
Micro Sensing Device Data Book
- English
Sensors Selector Guide
- English
Photomicrosensors Selection Guide
- Japanese
データシート

Appearance | Sensing method |
Connecting method |
Sensing distance | Aperture size H x W (mm) |
Output type |
Power supply voltage |
Operating mode |
Model |
---|---|---|---|---|---|---|---|---|
![]() |
Transmissi ve (slot type) |
Connector | 5 mm (Slot width) |
Emitter 1.4 × 1.4 Detector 1.4 × 0.5 |
Photo IC | 24 VDC | Dark-ON | EE-SX3173-P3-Z |
Light-ON | EE-SX4173-P3-Z | |||||||
5 VDC | Dark-ON | EE-SX3173-P2 | ||||||
Light-ON | EE-SX4173-P2 |
Models available
Power supply voltage: In addition to the conventional 5 VDC supply, model also available with 24 VDC supply best for large devices | Mounting: New model available with M3 screws | |
![]() |
| ![]() |
Downsizing Smallest class in the industry *: Downsizing of products with unique optical elements is realized * As of August 2018, according to research by our company |
Environment resistance Connection: Equipped with connectors with locks for resistance against vibration and shock |
|
![]() |
| ![]() |
Application Examples

Item | Symbol | Rated value | Unit | Remarks | |
---|---|---|---|---|---|
EE-SX3173-P3-Z EE-SX4173-P3-Z |
EE-SX3173-P2 EE-SX4173-P2 |
||||
Power supply voltage |
VCC | 26.4 DC | 5.5 DC | V | - |
Output voltage | VOUT | 26.4 | 13.2 | V | - |
Output current | IOUT | 16 | mA | - | |
Permissible output dissipation |
POUT | 80 | mW | Fig 1. | |
Operating temperature |
Topr | -25~+55 | ℃ | * | |
Storage temperature |
Tstg | -30~+80 | ℃ | * | |
Soldering temperature |
Tsol | - | ℃ | - |
Electrical and Optical Characteristics (Ta = 25°C)
Item | Symbol | Value | |
---|---|---|---|
24 VDC model | 5 VDC model | ||
Dark-ON | EE-SX3173-P3-Z | EE-SX3173-P2 | |
Light-ON | EE-SX4173-P3-Z | EE-SX4173-P2 | |
Power supply voltage |
VCC | 24 ±10%V Ripple (p-p) 10% |
5 ±10%V Ripple (p-p) 10% |
Current consumption |
ICC | 15 mA max. (With and without incident) |
25 mA max. (With and without incident) |
Low-level output voltage |
VOL | 0.3 V max. (IOUT = 16 mA) (Dark-ON: Without incident, Light-ON: With incident) |
|
High-level output voltage |
VOH | (Vcc x 0.9 V min. (VOUT = VCC, RL = 47 kΩ)) (Dark-ON: With incident, Light-ON: Without incident) |
|
Sensing object | − | 1.4 × 0.5 min. *1 | |
Response frequency |
f | 3kHz min. (VOUT = VCC, IOUT = 16 mA *2) |
|
Operating ambient light |
− | 1000 lx max. *3 | |
Peak emission wavelength |
λP | 855nm | 940nm |
*2. The value of the response frequency is measured by rotating the disk as shown below.

*3. When fluorescent light is used.
Exterior Specifications
|
L-shaped mounting | |||||||||
---|---|---|---|---|---|---|---|---|---|---|
EE-SX3173-P3-Z EE-SX4173-P3-Z EE-SX3173-P2 EE-SX4173-P2 |
||||||||||
Connecting method | Connector | |||||||||
Weight | Approx. 1.5 g | |||||||||
Materials | Case | Polybutylene terephthalate (PBT) | ||||||||
Emitter/ receiver |
Polyphenylene sulfide (PPS) fiber |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Correct Use
Mounting
- 1.This product is intended to be built into devices so no special measures have been taken against external light interference. When using a DC light sensor in an area exposed to an incandescent lamp or other external light interference, it should be mounted so that the effects of external light interference can be avoided.
- 2.Mount the sensor securely on a flat surface.
- 3.Use M3 screws to secure the Photomicro Sensor (use together with spring washers and 6-mm-diameter flat washers to prevent screws from loosening). Use a tightening torque of 0.54 N·m max.
- 4.Take care that nothing comes into contact with the sensing element of the sensor. Damage to the sensing element will result in poor performance.
- 5.Before using the sensor, check to make sure that it has not become loose due to vibration or shock.
Wiring
Surge Prevention
- 1.If there is a surge in the power supply, try connecting a Zener diode (ZD with a voltage of 30 to 35 V) or a capacitor (with a capacitance of 0.1 to 1 ?F), depending on the operating environment. Use the sensor only after confirming that the surge has been removed.
- 2.Do not use a small inductive load, such as a relay.
- 3.If photomicrosensor wires are placed in the same tubes or ducts as high-voltage lines or power lines, induction may cause malfunction or damage. Either wire the photomicrosensor separately or place the wires in separate tubes.
- 4.Make sure that connectors (commercially available) are securely locked.
Voltage Output
A sensor with an open collector output can be connected to a counter with a voltage input by connecting a resistor between the power supply and output. Select a resistor with reference to the following example. The resistance of the resistor is normally 4.7 kΩ. The wattage of the resistor is 0.5 W at a power supply voltage of 24 V.
- 1.A sensor with an open collector output can be connected to a counter with a voltage input by connecting a resistor between the power supply and output. Select a resistor with reference to the following example. The resistance of the resistor is normally 4.7 kΩ. The wattage of the resistor is 0.5 W at a power supply voltage of 24 V.
Example: EE-SX4173-P3-Z
When inserting a load resistor (R = 5.6 kΩ) in the following device
- Counter Specifications
-
Input impedance 5.6 kΩ Voltage judged as high level (input ON) 4.5 to 30 VDC Voltage judged as low level (input OFF) 0 to 2 VDC The high and low levels are found using the following formulas. The input device specifications must satisfy both formulas.
High level:
Note: Refer to the ratings of the sensor for the residual voltage of the load current.
Handling during Wiring
- 1.If a force is applied to the connection area between the terminal and connector by bending or pulling the cable after the wiring is completed, the connector contact part or connection area with the cable may be damaged, resulting in contact failure. Make sure that a stress (external force) as shown in the figure below is not applied to the connection area between the terminal and connector when routing and connecting cables or harnesses.
- 2.Do not perform cord wiring when power supply voltage is applied. Doing so may result in damage.
Other Precautions
Make sure the total length of the power cable connected to the product is less than 10 m.
Design
Design should be made so that light is completely shut off during operation. We recommend that sensing objects are made of metal.
(With an infrared light sensor, infrared light will pass through the sensing object made of resin, resulting in unstable detection.)
Connection with PLC (NPN Open Collector Type)
Mounting should be carried out by reference to the figure below.
Connection with Counter (NPN Open Collector Type)
Mounting should be carried out by reference to the figure below.
- 1.Non-voltage input
- 2.Transistor input (voltage input)
Others
- 1. Do not connect or disconnect the connector while power is applied. Doing so may result in breakage.
- 2. Do not mount the sensor in the following places because doing so may cause malfunction or damage.
- 1) Places exposed to dust or oil mist
- 2) Places exposed to corrosive gas
- 3) Places directly or indirectly exposed to water, oil, or chemicals
- 4) Outdoor or places exposed to intensive light, such as direct sunlight
- 5) Make sure that the operating ambient temperature is within the rated range.
- 3. The sensor may be dissolved by exposure to organic solvents, acid, alkali, aromatic hydrocarbon, and chlorinated aliphatic hydrocarbon solvents, causing deterioration in the characteristics. Do not expose the sensor to such chemicals.
- 4. An output pulse may occur when the power supply is turned ON depending on the power supply and other conditions. Use the sensor in the stable ready-for-detection state reached in 100 ms after turning on the power supply.