Product Details Portlet
2SMPP-02 MEMS Gauge Pressure Sensor
MEMS Gauge Pressure Senser Featuring Small Size and Low Power Consumption
- Ultra-miniature 6.1 × 4.7 × 8.2 mm (L × W × H).
- Superior electrical characteristics
to capacitive type pressure sensers. - 0 to 37 kPa pressure range.
Offset voltage of -2.5±4 mV
Span voltage of 31.0±3.1 mV - Low Power consumption of 0.2 mW
- Low Temperature Influence
Span of ±1.0%FS
Offset of ±3.0%FS
RoHS Compliant
- English
Datasheet
- English
User’s Manual
- English
Sensors Selector Guide
- Japanese
データシート
- Chinese
目录

Note: This web page provides an excerpt from a datasheet. Refer to Product Datasheet and other applicable documents for more information.
Model | Classification | Structure | Packaging |
---|---|---|---|
2SMPP-02 | Bottom Port Type | SOP | Plastic sleeve |
Item | 2SMPP-02 |
---|---|
Type of pressure*1 | Gauge pressure |
Sensing method*2 | Piezoresistance |
Pressure medium | Air |
Driving method | Constant current drive |
Drive current | 100 μA DC |
Pressure range | 0 to 37 kPa |
Withstand pressure | 53 kPa |
Absolute maximum current | 130 μA DC |
Ambient operating temperature | 0 to 50°C (with no condensation or icing) |
Ambient operating humidity | 15% to 95% (with no condensation or icing) |
Ambient storage temperature | -30 to 85°C (with no condensation or icing) |
Ambient storage humidity | 10% to 95% (with no condensation or icing) |
Weight | 0.17 g |
Note: The above specifications are the results of measurements taken at an ambient temperature of 23°C. *1 Do not use the Sensor under negative pressure. *2 Do not use any corrosive gases. Use only air. |
Item | 2SMPP-02 |
---|---|
Bridge resistance | 20±2kΩ |
Offset voltage | -2.5±4.0mV |
Span voltage | 31.0 ±3.1 mV (with an applied pressure of 37 kPa) |
Non-linearity | Max.0.8%FS(0~37kPa) |
Pressure hysteresis | 0.5% FS (0 to 37 kPa) |
Temperature influence of span voltage | 0.5±1.0%FS(0°C) |
0.3±1.0%FS(50°C) | |
Temperature influence of offset voltage | 0±3.0%FS(0~25°C) |
0±3.0%FS(25~50°C) |
Measurement conditions: Ambient temperature = 23°C, constant current and drive current = 100 μA |
(unit: mm)
![]() Note: Unless otherwise specified, the tolerance for all of the above drawings is ±0.3 mm. |
Precautions for Correct Use
Handling the Sensor
(1) Air is the only pressure medium that may be used directly with the Sensor. Do not use corrosive gases (organic solvent gases, sulfurous gases, hydrogen sulfide gas, etc.) or pressure mediums containing water particles. These pressure mediums may cause malfunctions.
(2) The Sensor is not drip-proof. Do not use the Sensor in any environment where it may be subjected to water or other liquids.
(3) Do not use the Sensor in any environment where condensation may occur. If moisture freezes on the Sensor chip, variations may occur in the Sensor output or the Sensor may malfunction.
(4) Do not insert wires, pins, or any other foreign objects into the connecting tube. Doing so could destroy the pressure sensor chip inside the Sensor, or the foreign object may become stuck inside the connecting tube and affect the Sensor output.
(5) Always stay within the rated pressure range. Using a pressure outside of this range may damage the Sensor.
(6) Do not use the Sensor in any environment subject to vibration from ultrasonic or high-frequency waves.
(7) The Sensor output may be affected if the pressure sensor chip is exposed to light. Do not expose the Sensor chip to light.
(8) Static electricity may destroy the Sensor. Any charged materials or surfaces, such as workbenches, floors, or technicians, must be properly grounded to prevent static electricity.
(9) Applying excessive force to the pins may deform them and damage the soldering. Do not drop the Sensor and always handle it with care. Do not use the Sensor in any environment that is subject to excessive steam or dust.
(10) Refer to the connection diagrams when connecting the pins on the Sensor.
(11) Do not connect to the pins on the Sensor in the wrong direction. Doing so may cause variations in Sensor output or malfunctions.
(12) External noise may effect the Sensor output. Take any necessary measures to eliminate external noise.
(2) The Sensor is not drip-proof. Do not use the Sensor in any environment where it may be subjected to water or other liquids.
(3) Do not use the Sensor in any environment where condensation may occur. If moisture freezes on the Sensor chip, variations may occur in the Sensor output or the Sensor may malfunction.
(4) Do not insert wires, pins, or any other foreign objects into the connecting tube. Doing so could destroy the pressure sensor chip inside the Sensor, or the foreign object may become stuck inside the connecting tube and affect the Sensor output.
(5) Always stay within the rated pressure range. Using a pressure outside of this range may damage the Sensor.
(6) Do not use the Sensor in any environment subject to vibration from ultrasonic or high-frequency waves.
(7) The Sensor output may be affected if the pressure sensor chip is exposed to light. Do not expose the Sensor chip to light.
(8) Static electricity may destroy the Sensor. Any charged materials or surfaces, such as workbenches, floors, or technicians, must be properly grounded to prevent static electricity.
(9) Applying excessive force to the pins may deform them and damage the soldering. Do not drop the Sensor and always handle it with care. Do not use the Sensor in any environment that is subject to excessive steam or dust.
(10) Refer to the connection diagrams when connecting the pins on the Sensor.
(11) Do not connect to the pins on the Sensor in the wrong direction. Doing so may cause variations in Sensor output or malfunctions.
(12) External noise may effect the Sensor output. Take any necessary measures to eliminate external noise.
Transportation and Storage
(1) Do not store the Sensor in any environment that contains corrosive gases (organic solvent gases, sulfurous gases, hydrogen sulfide gas, etc.).
(2) The Sensor is not drip-proof. Do not store the Sensor in any environment where it may be subjected to water or other liquids.
(3) The cardboard packaging will deteriorate over time depending on the humidity, number of boxes stacked on top, and other factors. Follow the first in, first out rule for storage. Do not drop or throw the Sensor. Handle it with care.
(4) If the inner packaging is dropped, the stopper may be dislodged from the tube causing the Sensor to fall out and become damaged.
(5) The surface of the tube containing the Sensor is coated in a film to prevent static electricity. Observe the following items regarding this protective coating:
1. Avoid exposure to water, which may wash away the protective coating.
2. The protective anti-static electricity coating may be sticky to the touch in high-temperature, high-humidity environments. 3. The protective anti-static electricity coating degrades over time. Do not store the Sensor for more than 6 months. Also, do not reuse the packaging.
(6) Store the Sensor in an environment with suitable temperature and humidity levels. Temperature: 5 to 30°C, Humidity: 40% to 60%
(7) Leads are silver-plated and may change color over time depending on the storage conditions. Discoloration after the Sensor is delivered is not covered under warranty. Be sure to store the Sensor under the proper conditions.
(8) Do not store the Sensor in any environment with excessive steam or dust.
(2) The Sensor is not drip-proof. Do not store the Sensor in any environment where it may be subjected to water or other liquids.
(3) The cardboard packaging will deteriorate over time depending on the humidity, number of boxes stacked on top, and other factors. Follow the first in, first out rule for storage. Do not drop or throw the Sensor. Handle it with care.
(4) If the inner packaging is dropped, the stopper may be dislodged from the tube causing the Sensor to fall out and become damaged.
(5) The surface of the tube containing the Sensor is coated in a film to prevent static electricity. Observe the following items regarding this protective coating:
1. Avoid exposure to water, which may wash away the protective coating.
2. The protective anti-static electricity coating may be sticky to the touch in high-temperature, high-humidity environments. 3. The protective anti-static electricity coating degrades over time. Do not store the Sensor for more than 6 months. Also, do not reuse the packaging.
(6) Store the Sensor in an environment with suitable temperature and humidity levels. Temperature: 5 to 30°C, Humidity: 40% to 60%
(7) Leads are silver-plated and may change color over time depending on the storage conditions. Discoloration after the Sensor is delivered is not covered under warranty. Be sure to store the Sensor under the proper conditions.
(8) Do not store the Sensor in any environment with excessive steam or dust.
Mounting Method
Mount the Sensor on the land pattern of a printed circuit board.
Solder pin 2 securely to the printed circuit board in order to maintain the mechanical strength of the mounted Sensor.
Solder pin 2 securely to the printed circuit board in order to maintain the mechanical strength of the mounted Sensor.
Soldering Method
Due to its small size, the heat capacity of the Sensor is limited. Therefore, measures must be taken to minimize the effects of heating from external sources. Solder bath submersion: 260°C max. for 10 seconds max.
Soldering iron: 260°C max. for 10 seconds max.
Apply heat to the Sensor pins only, and not to the Sensor package. Do not use any flux that may release corrosive gases. Do not allow any flux to enter the inside of the case.
Soldering iron: 260°C max. for 10 seconds max.
Apply heat to the Sensor pins only, and not to the Sensor package. Do not use any flux that may release corrosive gases. Do not allow any flux to enter the inside of the case.
Cleaning
Do not allow any cleaning liquid to enter the inside of the case.
Do not use ultrasonic cleaning. Doing so may break connections.
Do not use any cleaning liquids that contain silicone. Such cleaning liquids may remain on the surface of the Sensor.
Do not use ultrasonic cleaning. Doing so may break connections.
Do not use any cleaning liquids that contain silicone. Such cleaning liquids may remain on the surface of the Sensor.
Coating
Do not apply any coating to the Sensor.