RoHS compliance status / Certificate of Non-inclusion download
Data Update Date: Aug 08th 2022
Search results
Product Category | Type | Model | Compliance status*1 | Download List*2 |
---|---|---|---|---|
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC3 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC5 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC12 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC24 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC3 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC5 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC6 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC12 | ![]() |
Login/Register |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC24 | ![]() |
Login/Register |
China RoHS ○ × Table *1 | |||||||||
---|---|---|---|---|---|---|---|---|---|
Product Category | Type | Model | Lead(Pb) | mercury(Hg) | cadmium(Cd) | hexavalent chromium(Cr(VI)) | polybrominated biphenyls(PBB) | polybrominated diphenyl ethers(PBDE) | Environmentally Friendly Use Period*2 |
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC3 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC5 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC12 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US DC24 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC3 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC5 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC6 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC12 | |||||||
STANDARD POWER RELAY | G6CU | G6CU-1117P-US-P6C DC24 |
Management Criteria for Regulated Chemicals
For issuance of our “Certificate for Non-inclusion of Chemical Substances in Products/Materials”, the following criteria apply to prohibited chemicals.
Management Criteria for Regulated Chemicals (Ver. 4.8) <PDF 1.3MB>
- *1: Compliance status
- The Ro mark
in the datasheet indicates that products of this product model do not contain any of the 10 chemicals restricted under EU RoHS.
This mark shows that Omron can deliver RoHS-compliant products for this model, and does no necessarily mean that all the products of this model are compliant with RoHS.
Some existing stock products may not be RoHS-compliant depending on the purchase date.*EU RoHS Directive: (ten restricted substances and their respective maximum levels:
Lead (Pb) : 1,000 ppm, Mercury (Hg): 1,000 ppm, Cadmium (Cd) : 100 ppm, Hexavalent chromium (Cr(VI)) : 1,000 ppm, Polybrominated biphenyls (PBB) : 1,000 ppm, Polybrominated diphenyl ether (PBDE) : 1,000 ppm, Bis(2-ethylhexyl) phthalate (DEHP or DOP) : 1,000 ppm, Butyl benzyl phthalate (BBP) : 1,000 ppm, Dibutyl phthalate (DBP) : 1,000 ppm, and Diisobutyl phthalate (DIBP) : 1,000 ppm The above restrictions do not apply to items exempted by the RoHS Directive. We have confirmed that the four phthalates are not intentionally used in our products over the threshold value. - The Ro mark
- *2 Downloading of Certificate of Non-inclusion
- You can download Certificate of Non-inclusion which certifies that the product does not contain chemical substances/substance groups restricted by Omron.
*Please contact us or distributors for products that are not found on e-web.
- *1: China RoHS Hazardous Substance Table
- [○] indicates that the concentration level of the restricted chemical in the homogeneous material is lower than the maximum limit value specified under China RoHS.
- [X] indicates that the concentration level of the restricted chemical in the homogeneous material is above the maximum limit value specified under China RoHS.
- If it is blank, the concentration levels are not confirmed yet. Please contact our sales representatives.
*China RoHS six restricted substances and limitation (GB/T26572)
Lead (Pb) : 1,000 ppm, Mercury (Hg): 1,000 ppm, Cadmium (Cd) : 100 ppm, Hexavalent chromium (Cr(VI)) : 1,000 ppm, Polybrominated biphenyls (PBB) : 1,000 ppm, and Polybrominated diphenyl ether (PBDE) : 1,000 ppm - *2 Environmentally-Friendly Use Period (EFUP)
- [e] indicates that the product does not contain any of the restricted chemicals over the maximum concentration limits.
- [10] indicates a EFUP in units of years (10 years), during which the product will not leak hazardous substances or cause any severe impact on the environment under normal conditions of use.
- If it is blank, the concentration levels are not confirmed yet. Please contact our sales representatives.
*Please contact us or distributors for products that are not found on e-web.